AXIS#.MOTOR.RSOURCE

Description

This parameter defines the type of source channel used to connect the motor thermal resistor, if one is present. The thermal resistor may be connected to the drive using a discrete wire or digital feedback channel:

AXIS#.MOTOR.RSOURCE Connection Type
0 Discrete wire
1 Digital feedback

If AXIS#.MOTOR.RSOURCE = 0, the temperature sensor is wired directly from the motor to the drive, and the drive calculates the temperature from the measured resistance.

If AXIS#.MOTOR.RSOURCE = 1, the temperature calculation happens at the feedback device and the temperature is provided to the drive using the feedback interface. The following feedback types support the digital temperature channel:

  • SFD Gen 2
  • SFD Gen 3
  • HIPERFACE DSL
  • EnDat Digital

If AXIS#.MOTOR.AUTOSET = 0, the user may set AXIS#.MOTOR.RSOURCE. However, if the value is set to 1 and the feedback does not support a digital temperature channel, the drive computes the temperature using the discrete connection method.

See Motor Temperature View.

Versions

Action Version Notes
Implemented 02-05-00-000

 

General Information

Type

Read/Write

Units

N/A

Range

0 to 1
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
AXIS1.MOTOR.RSOURCE

500bh

22h

Unsigned8

-

-

Read/Write

No

AXIS2.MOTOR.RSOURCE

510bh

22h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.RSOURCE

6243

1863

Unsigned8

Read Only

-

AXIS2.MOTOR.RSOURCE

71779

1186

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.RSOURCE

6243

Unsigned8

Read Only

-